Driving without a human driver is not a new idea. Ever since cars were invented, mankind has dreamt of self-driving cars or driverless cars. However, these dreams have so far not come true and automated vehicles have not been deployed on our roads. Not yet, at least.
Nowadays, this situation seems to be rapidly changing as the technology needed for automated driving is starting to become available. At the same time, there is increasing societal and political pressure to solve the problems related to human driven cars - such as traffic accidents, pollution and congestion. Many car makers already have prototypes of automated vehicles on the road today, and commercial market introduction doesn’t seem far away. Or does it?
Automated driving systems consist of complex technology. Various different sensor technologies - such as radar, camera, lidar and V2X communication – should provide a complete image of what is going on around the vehicle. This can only be reliably done with very advanced sensor data processing algorithms. Sophisticated decision and control algorithms then have to make sure the car reacts correctly to the practically infinite amount of events that can happen in real-world traffic.
But how to design, validate, and certify these automated driving systems? Which scenarios should be tested until a system can be released? How many kilometers need to be driven to prove that a system is robust and fail-safe? When is a system “good enough”? And should we re-test all scenarios after a hardware- or software-update? Even though there is no general consensus yet about the answers to these questions, it is clear that relying on traditional test-methods (i.e. road testing and test-track testing) will lead to a time-consuming and cost-intensive process.
TASS International’s vision is that the most effective way to develop and validate automated driving systems is by using a combination of simulation, laboratory experiments and real-world testing. Simulation results are used to define the physical experiments, whereas experimental results are used to validate the simulations. Our methodology and tool-suite enables our customers to validate automated driving systems at a much earlier stage and for much smaller investments. In addition to this, TASS International also provides a wide range of engineering and consultancy services for automated vehicle development.
" The PreScan software is used at VisLab during the algorithm design phase of our autonomous vehicles. Its usage allowed us to make very fast design iterations and contributed to a robust algorithm design and a successful road demonstration of our autonomous vehicles (www.vislab.it/proud). "
The complexity in cooperative and automated vehicles increases exponentially compared to traditional vehicles. An integrated tool suite supporting the full development V-cycle is crucial to enable cost and time efficient development processes. For the development phase we offer a state-of-the-art simulation platform called PreScan for developing active safety systems, automated driving systems and connected vehicle systems . Ranging in scale from complex traffic networks, down to component level simulations tools. For testing, hardware in the loop testing is necessary for sensor and communication systems, while a dedicated test environment for rapid, safe and reproducible testing of cooperative and automated vehicles is required to test complete systems. Finally, for validation and performance testing, a test site for urban, interurban and highway traffic is available.
Download our Automated Driving datasheet.
PreScan provides a physics-based simulation platform to prototype, test and validate your new advanced driver assistance systems (ADAS) and connected vehicle systems (V2X). Test and validate your Adaptive Cruise Control (ACC), Aumatic Emergency Braking (AEB) and Lane Departure Warning (LDW) systems.
Read moreMADYMO is the worldwide standard software for analysing and optimizing occupant safety designs. It is without rival for its accuracy, efficiency and versatility.
Read moreDelft-Tyre is a range of products and services to model tyre behaviour for vehicle dynamic simulations. Delft-Tyre provides an integral, cost efficient and fast tyre modelling for al simulation applications.
Read moreVehicle Hardware in the Loop, in short VeHIL, allows developers to test and evaluate the functionality of a complete vehicle, as well as its subsystems and sensors, in controlled yet realistic circumstances.
Read moreOur test facilities range from desktop simulation software, indoor laboratory testing to the A270/N270 public highway for large-scale outdoor testing. Test and validate connected vehicle systems & applications or evaluate your Intelligent Transport Systems (ITS) for effectiveness.
Read moreDedicated and customer focused solutions using global engineering capability. With over 30 years of experience in facing automotive challenges and strong partnerships with renowned institutes.
Read more