新闻动态

信息中心

- 产品

TASS International releases PreScan V8.5

TASS International is proud to announce the release of PreScan, version 8.5. PreScan is the leading physics-based simulation platform for the development, testing and validation of ADAS applications and autonomous driving.

This release introduces a number of exciting new features:

  • PreScan can now run natively on an ETAS real-time platform
  • Visual sensors that send an image to Matlab can run up to 70% faster
  • Data Model API can be used to create multiple scenarios based on different PreScan objects and scenarios
  • Data Model API can now generate abstract objects and calibration elements
  • Support for importing traffic lights and traffic signs defined in OpenDrive roads

 

Read the full list of new features and enhancements of PreScan V8.5, more general information about Automated Driving and ADAS physics-based simulation platform PreScan or request a free trial of PreScan.

请填写此下载表格