MADYMO

What's new in MADYMO?

   

MADYMO 7.8 & Workspace 7.8

On this webpage you can find information on what has been updated in MADYMO in the latest release as well as in the Workspace updates. Please contact us if you need more information. You can download the software in our protected download site.

 

Please fill in this download form

The new Simcenter Madymo release 7.8 brings a range of new features and improvements for all users across the entire suite of products. These include:

Benefits

  • Robustness: improved handling of large amounts of time history output
  • More robust partitioning for FE-FE contact definitions
  • Enhanced error handling of contact definitions
  • Reduced Solver XML parsing times
  • Enhanced stability: code updates carried out and libraries have been updated
  • Improved user experience: enhanced handling of DEFINE variables
  • Seat belt fitting enhancements
  • Version 3.1 of Active Human Model
  • THOR: US-NCAP and EuroNCAP versions are now included
  • Hybrid III family updated for improved regulatory compliance

Simcenter Madymo Workspace V7.8

Simcenter Madymo Workspace V7.8 contains the following new features.

General

  • A large number of updates have taken place under the hood to make the Workspace suite of tools ready for the future and future proof
  • Docking of windows is extended: dragging windows makes them dock easily or switch to tabbed layout
  • The icon menu bar will initially show collapsed, but will remember its latest configuration and reopen as closed in the previous session

XMADgic

  • Enhanced handling of DEFINE variables
  • Seat belt fitting enhancements
  • Enhancements in CAD model overlay
  • Dummy positioning enhancements
  • Recognition of closed chains in Madymo input deck
  • Active Human Initializer tool to import joint DOF and muscle activation values from settling simulation results. 

Coupling Assistant

  • Support for user-encrypted Madymo model content
  • Support for parameterized LS-DYNA input decks

MADPost

  • Additional pane layouts
  • Support for loading STEP files
  • Faster parsing of models with user encrypted content
  • Reduced memory usage for parsing of lengthy XY_PAIR tables

Solver performance

  • Overall solver speed up for Linux platforms
    • Upgrade from PGI to Intel compilers
Madymo v7.8 MADPost

Simcenter Madymo Solver V7.8

Simcenter Madymo Solver release 7.8 contains the following new features:

New feature

  • INJURY.IFD implemented, providing iliac force drop output according Euro NCAP specifications (TB 021)
  • The Iliac Force Drop (IFD) criterion is used by Euro NCAP as a measure to detect seat belt slip-off from the iliac wings of the ATD / crash dummy, which is considered to result in so called "submarining".
  • In case IFD criterion indicates that submarining has occurred (IFD value > 1000 N), this should be confirmed by viewing the dummy kinematics
  • Iliac Force Drop Criterion is implemented in Madymo as INJURY.IFD
    • IFD value written to .peak and .pkx files
    • IFD(t) time history signal written to .injury file

Parser Performance 

  • Overall parser speed up, most significantly for Linux platforms
  • Faster parsing of models with large numbers of DEFINE variables
  • Faster parsing of models with user encrypted content
  • Reduced memory usage for parsing of lengthy XY_PAIR tables

Solver performance

  • Overall solver speed up for Linux platforms
  • Upgrade from PGI to Intel compilers
EuroNCAP logo

Simcenter Madymo Occupant Models V7.8

Simcenter Madymo release 7.8 contains the improvements to the following occupant models:

Dummy modelbase nameprevious versionversion in R7.8 installer
Hybrid-III 5th femaled_hyb305el2.02.1
 d_hyb305fc2.42.5
Hybrid-III 50th maled_hyb350el2.02.5
 d_hyb350fc4.34.3.1
Hybrid-III 95th maled_hyb395el1.41.4.1
 d_hyb395fc1.11.1.1
THOR 50th male (US)d_thor50el3.0.13.1
 d_thor50fc-3.1 (new)
THOR 50th male (EU)d_thor50el_hyb3lx3.0.13.1
 d_thor50fc_hyb3lx-3.1 (new)
WorldSID 50th maled_ws50lhfc_Q4.04.1
 d_ws50rhfc_Q4.04.1
Hybrid-III 6YO childd_hyb36yel2.102.11
Q6 6YO childd_q06yel1.41.5
Q10 10YO childd_q10yel2.12.2

 

 

 

 

 

 

 

 

 

 

 

 

 

Human modelbase nameprevious  versionversion in R7.8 installer
Active human 50th maleh_act50fc_sitting2.03.1
 h_act50fc_standing2.03.1
Human pedestrian familyh_ped3yel5.15.2
 h_ped6yel5.15.2
 h_ped05el5.15.2
 h_ped50el5.15.2
 h_ped95el5.15.2
Human pedestrian scalableh_ped50el.par5.15.2

 

 

 

 

 

 

 

 

 

Application modelbase nameprevious versionversion in R7.8 installer
Integrated safety - drivera_act50fc_is_drv_settling2.13.1
 a_act50fc_is_drv2.13.1
Integrated safety - passengera_act50fc_is_psg_settling2.13.1
 a_act50fc_is_psg2.13.1

 

Image Gallery

madymo throughput times
A typical set of 47 simulations now takes 21.8 hrs with R7.8 as opposed to 30.5 hours in R7.7
Elapsed simulation time vs simulated event duration
Typically a 3 second simulation has improved by almost 1 hour and now takes only 2 hours in R7.8
d_hyb305el_q_yaris
Madymo Active Human Model
Madymo Active Human standing
  • madymo throughput times
  • Elapsed simulation time vs simulated event duration
  • d_hyb305el_q_yaris
  • Madymo Active Human Model
  • Madymo Active Human standing

Previous releases of MADYMO

The MADYMO product suite is updated at regular intervals. Check out previous releases and their content.

The MADYMO product suite consists of the following products: Solver (stand alone and coupling), Dummy, Human and Pedestrian models and a set of dedicated pre- and post processing tools.