PreScan

What's new in PreScan?

   

What's new in PreScan?

Information about new features and enhancements in the latest PreScan releases.

Please fill in this download form

PreScan 2019.2

  • Launch 1.0 of Matlab Data Model API
    • Allows for rapid parameter variation
    • Allows for an automatic way of executing large number of scenarios and data collection
    • Allows creation of scenarios via Matlab scripts
  • Ground truth outputs for the Unreal Physics Based Camera
    • Provides pixel by pixel correlation to the Unreal Physics based camera taking into account lens distortions
    • Distance: Provided in meters
    • Segmentation: Provided as object IDs, object type IDs, or a combination of both
    • Optical Flow: Tracks movement/motion of pixels in between frames
  • Physics Based Radar
    • Support for Optix 6 now provides significant speed improvements
    • Minor bug fixes
Ground Truth Outputs for Unreal Physics Based Camera
Ground Truth Outputs for Unreal Physics Based Camera

PreScan 2019.1

  • New Unreal Physics based camera
    • Complete sensor & optics pipeline simulation
    • Fisheye camera simulation
    • Support for rain simulation
    • Improved performance (compared to original Physics Based Camera)
  • Additionally, the use of the Unreal Gaming Engine provides the following advantages:
    • Improved shadows
    • Improved reflections
    • Improved shading
    • Improved motion blur
    • Improved grass models
  • New Physics Based Radar model
    • This new Physics Based Radar model allows users to generate raw data output (e.g. ADC data) to help with the testing and development of signal processing algorithms, and new automotive radar systems.
    • Validation of this new radar model has been performed with Tier 2 and Tier 1 manufacturers
  • New Object List Provider
    • Provides a filterable list of all the objects in the scene using global coordinates
  • Improved OpenDRIVE support
    • Pedestrian crossings
    • Stop lines
    • Constant roadshape
    •  Asphalt crossing
  • Additionally, the following sensors now work in conjunction with OpenDRIVE roads:
    • ISS
    • ALMS
  • Matlab Data Model API 0.9:
    • AIR sensor support (creation of the sensor, modification functions, business layer)
    • Creation of Generic Models
    • Trajectory related auxiliary functions
      • Getting length of a path
      • Getting pose at a distance
    • Get list of WorldObjects
    • New “Run with data models function”
New physics based camera sensor based on unreal
New Physics Based Camera Sensor Based on Unreal Engine

PreScan V8.6

  • New CIDAS importer available
    • China In-Depth Accident Study (CIDAS) plugin is now available
    • Able to import accident scenes easy and fast for testing and development of ADAS and AV functionality
  • Point Cloud Sensor updates
    • The following outputs are now available:
    • Object ID
    • Doppler Velocity
    • Angle information
  • Data Model API updates
    • The following outputs are now available: Vehicles, nature elements, information boards, and highway overhangs
    • The following objects can now be modified: Trajectories (Path & Speed Profile) and traffic signs
  • OpenDRIVE updates
    • Parameters of an imported OpenDRIVE road can now be modified via the Property Editor
  • Sensor detectability updates
    • Objects can now be configured to be Invisible, Occluding, or Detectable for Prescan sensors
Prescan Unreal sensor

PreScan V8.5

  • ETAS Support
    • Native support for real-time ETAS hardware platform
    • The following sensors can run natively: AIR, ALMS, LMS, Wheel Contact, Radar, Lidar, Ultrasonic, TIS, BRS, Collision Detection
  • Better run-time performance
    • Visual sensors that send an image to Matlab/Simulink now have up to 70% better run-time performance
  • Data Model API updates
    • Component based modelling is now possible
    • Support for abstract objects and calibration elements
  • OpenDrive support
    • Traffic lights can be imported
    • Traffic signs can be imported
    • Imported lane types are now shown with different colors
  • 3D dynamics for trucks
    • The following truck models have been updated with 3D dynamics: DAF 95, DAF Euro 6, Volvo FH16, Nissan Cabstar
Prescan evasive maneuver scenario
Evasive maneuver scenario

PreScan V8.4

  • Point Cloud Sensor
    New generation sensor for simulation of point clouds for real time LIDAR applications
    • Sensor measurements are given in x,y,z coordinates or as a range
    • Sensor can provide an intensity value for each point
  • Matlab SLX file format
    • PreScan experiments now use the Matlab SLX format as the new default
  • OpenDrive import functionality
    • Support for banking (superelevation)
    • Support for different lane markings
    • Support for vehicle lane changes (once a road has been imported)
  • Frame skip feature
    • Visualization can be de-coupled from simulation to prevent slowdown in performance
PreScan Point Cloud Sensor
PreScan Point Cloud Sensor

PreScan V8.3

  • Data Model API
    • ​Data Model API allows customers to create scripts that can be used for test automation purposes
    • The API will give users access to the internals of a PreScan experiment and provide functions that will help users change parameters using a script
    • Through the API a user can now replace PreScan objects
    • Through the API a user can now replace delete PreScan objects
    • Through the API a user can now edit sensor configuration parameters
  • PreScan Cluster
    • PreScan experiments can now be packaged into Docker containers that can run on Linux operating systems
    • Docker containers can be distributed over a cluster to run simulations at scale
  • OpenDrive import functionality
    • Support for height information
    • Support for the ALMS and LMS sensors
    • Support for the Vissim plugin
  • Matlab compatibility
    • Matlab 2016a
    • Matlab 2016b
    • Matlab 2017b
OpenDrive support in PreScan now works with height elevation, Vissim, and LMS sensors

PreScan V8.2

  • PreScan Standalone Target (PSRT)
    • PSRT can now be used to generate a zip-file with experiment contents and allow users the flexibility to deploy experiments on different platforms/operating systems:
    • PSRT can run without Matlab/Simulink
    • PSRT can run in both Windows and Linux
    • PSRT can be used to run PreScan on cluster systems
    • PSRT can be used to run a fully standalone simulation on a Concurrent RedHawk system
  • OpenDRIVE support
    • ​Support for OpenDRIVE 1.4 roads
  • New Vehicle models
    • Improved visual details
    • Frame rates are up to 3 times faster when using a large number of vehicles
    • Level of Detail (LOD) technology is available on all vehicles
  • Vissim upgrade
    • Support for automatic generation of Vissim roads based on PreScan roads
New vehicle models
New vehicle models

PreScan V8.1

  • Image Segmentation Sensor:
  • The Image Segmentation Sensor (ISS) is a tool to generate semantically segmented images. It is useful in application domains such as classification, (deep) learning, pedestrian recognitions, collision avoidance.
  • The ISS will typically be used in combination with the Camera Sensor to obtain the image that is being segmented.
  • FMI/FMU support:

PreScan supports the FMI standard in two ways:

  • A PreScan Compilation Sheet can be converted to an FMU that can be simulated by another FMI simulator 
  • 3rd-party FMU's can be embedded inside a PreScan Compilation Sheet.
  • Generic Model Improvements:
  • Generic models now support 2D, 3D and userdefined vehicle dynamics: 
  • Generic models can be configured, modified and used similar to all other models within the PreScan editor.
  • Generic models without joints, lights or dynamics are no longer shown on the compilation sheet
  • Updated Infrastructure Models:
  • The building models have been updated, these new versions of existing PreScan models improve the visual appearance and performance.
  • General notes:
  • V2X plugin has been re-introduced
Image Segmentation Sensor - Segmented images for Deep Learning and Artificial Intelligence
Image Segmentation Sensor

PreScan V8.0

  • Real Time support:
  • The Simulink compilation sheet can be compiled and run on a Concurrent RedHawk Real-Time machine.
  • Performance improvement of the sensor and actuator blocks in Simulink:
  • All sensor and actuator blocks in Simulink are implemented as S-Funcions. Most of these S-Functions have less overhead and thus improve the performance of the simulation.
  • Simulink accelerated mode:
  • Simulink accelerated mode is now supported. The compilation sheet is first compiled and then run. This may increase initialization time, but improves the performance of the simulation. 
  • Model Preparation Tool:
  • The Model Preparation Tool (MPT) allows users to import 3D model files and prepare it for use in the PreScan editor
  • The following 3D model file formats are supported: .dea (COLLADA), .obj, .ive, .osg, .osgb, .osgt
  • Custom model features such as joints, joint groups, lights, sensor mounts, default sensor position, and default visuaid positions can be added
  • General notes:
  • Depth Camera has improved performance on scenarios that have active lights and shadows
  • FlexLM License has been upgraded to version 11.14.0
  • Support for Windows 10
Model Preparation Tool

PreScan V7.6

  • Updated Physics Based Camera plugin
  • Material improvements: Pre-defined materials, configuration of RGB colors on materials, reflections and retro reflections
  • Lighting improvements: Increased performance, quality improvements, support for a higher number of lights, and a new set of SPDs for vehicle and street lights
  • Traffic signs: New traffic signs, improved dutch and german signs, and new matrix signs with support for multiple SPDs and LED blinking
  • New test automation capabilities

Note: PBC Plugin update is available as a separate download. Please contact your Sales office for more information. 

  • Updated V2X plugin:
  • New communication model available: Physics based
  • Message types (BSM, CAM, DENM, generic) are now all fine-tunable 
  • Simulink V2X output is now completely typed 
  • New Vissim traffic simulation plugin
  • New Vissim plugin available in PreScan
  • The Vissim traffic simulation plugin enables users to do traffic simulation based on PTV Vissim 
  • Object Camera Sensor:
  • The Object Camera Sensor (OCS) has been ported to the PreScan Multiprocessing Architecture resulting in improved performance
  • During simulation, it will be run as a separate process
  • Multiple Object Camera sensors can be run in parallel
  • Small quality improvements are realized because of the migration to the new architecture
  • Bézier-/Flexroads:
  • Bézier- and Flexroads now support Z offset
  • Flexroad definition points now support Z offset, banking, and tilt
  • Various models have been added/updated:
  • Updated pedestrian models
  • New pedestrian models
  • New Lexus actors
  • New Toyota Prius actor
  • New DAF truck
  • New Volvo truck
  • New Lane Change Assistance System (LCAS) scenarios
Cloverleaf road interchange
Cloverleaf road interchange

PreScan V7.5

  • Collision Detection:
  • The collision detection functionality has been optimised in order to run at higher frame rates. This has been accomplished by putting the functionality in a separate process and by optimising the collision detection strategy.​
  • Depth Camera Sensor:
  • The depth camera sensor is re-implemented to profit from the multi-processor capabilities of PreScan. Multiple depth camera sensors are processed in parallel which results in a higher overall performance.
  • Fisheye Camera Sensor:
  • The fisheye camera sensor has been improved in a similar way as the camera sensor and the depth camera sensor. Therefore, the fisheye camera also profits from the multi-processor capabilities of PreScan resulting in higher performance.
  • Shadow quality:
  • An option has been added to set different levels of shadow quality for the camera related sensors and 3D viewer. The setting is saved per experiment.
  • GPU assignment for Camera Sensor and Fisheye Camera Sensor:
  • An option has been added to the assignment dialog of the camera sensor and fisheye camera sensor to run the sensor on a specific GPU. This makes full use of the capability of multiple GPUs in a single machine to allocate sensors on a specific GPU, resulting in a higher performance. Similar functionality will be available for the depth camera in a future release.
  • Improved Game Controller support:
  • The support for the Logitech G29 steering wheel has been added to the built-in game controller. Experiments with previous solutions with a separate sensor have become obsolete with this built-in functionality, and should be cleaned up.
PreScan V7.5 Improved Shadow Quality
Different Shadow Quality Settings

PreScan V7.4

  • New Bounding Rectangle Sensor:
  • run multiple bounding rectangle sensors in parallel which will result in decreased run time.
  • The quality of the sensor has been improved where possible and the new bounding rectangle sensor detects each sensor detectable object.
  • The new Bounding Rectangle Sensor focuses on its primary output: bounding rectangles. Therefore a convenience block (part of the 'Useful Blocks' in the Simulink library) is needed when the rectangles are needed in combination with the images from the Camera Sensor because the Bounding Rectangle Sensor does not output Camera Sensor-like images anymore.
  • Camera Sensor:
  • PreScan version 7.4.0 can run multiple camera sensors are run in parallel and will therefore result in decreased run time.
  • Also,  it is now possible to disable the viewer output while still sending output images to Simulink resulting in reduced simulation time.
  • Updated IBEO plugin:
  • The new IBEO plugin is now also capable of supporting ego vehicle lane changes since ego lane is detected and used for road generation. In previous versions of the plug-in ego vehicle lane changes would result in shifted road locations.
  • Also, the measured road width (at the beginning of the recording) is used throughout the simulated road.
  • General enhancements:
  • The remote viewer is now capable of running in a borderless window and can be positioned.  This allows rear-view mirror images to be modeled in driving simulator applications.
PreScan Bounding Rectangle Sensor
PreScan Bounding Rectangle Sensor

PreScan V7.3.0

  • Updated LIDAR and Ultrasonic sensor model

The LIDAR and Ultrasonic sensor have been ported to the PreScan Multi-Processing architecture:

  • During simulation it will be run as a separate process resulting in a better performance.
  • Usage of multiple sensors has improved. Multiple sensors can simulate in parallel instead of serially.
  • Noise has been added to the Ultrasonic sensor.
  • The Ultrasonic sensor's FOV and range are now configurable.
     
  • New analytical lane marker sensor

A new lane marker sensor has been added.  This sensor reports sets of polynomials describing the lane lines in the view of the sensor. A convenience block is added for the user to display the polynomials in Simulink.  The GPU is not used and therefore the sensor is much faster than the normal lane marker sensor.

  • Test Automation improvement

    Additional parameters can be set from the PreScan CLI using Test Automation with rebuild:

  • Traffic sign pole and plate dimensions
  • Traffic sign imperfection parameters
  • Explicit sun position and intensity
     
  • General improvements
  • It is now possible to disable the viewer in the Simulation Scheduler which significantly improves the simulation speed.
  • Simulation speed for scenarios with multiple pedestrians has been improved.
  • Matlab 2010b is the lowest Matlab version that is supported.  Matlab 2014 has been added as a officially supported version.
  • The IBEO plugin was updated to use the latest SDK interface from IBEO and can therefore use the latest IBEO format and functionality. 
  • A demo model for coupling with VI-grade is included in the installer.
  • Small AIR sensor updates.

 

PreScan V7.2.0

Scroll down for a video of the PreScan V7.2 update webinar.

  • Updated physics based camera sensor model
  • A user interface is made available to specify various camera settings:
    • Focal length and aperture
    • Vignetting
    • Modulation Transfer Function (MTF)
    • Barrel and Pincushion distortion
    • RGGB and RCCC color filter and custom transmission curves
    • Grid Layout
    • Various imager and electronic settings, and spectral response
    • A/D Conversion: digital precision and gain
    • Read noise, Dark noise and Photon dependent noise
  • Various stages of the image pipeline can be written to disc and the final camera sensor image can be send directly to Matlab/Simulink
  • Various default SPDs for vehicle and street lights (e.g. High/low pressure sodium, filament, LED, halogen, mercury)
  • New V2X statistical sensor model

The V2X Statistical Model Plugin is an extension to the existing Antenna system within PreScan. The Antenna system is used for Vehicle-to-Vehicle (V2V) and Vehicle-to-Infrastructure (V2I) communication. This plugin enhances the algorithm for determining whether a transmitted messages are successfully received by a receiver. Instead of a hard cut-off distance, a more realistic set of statistical models is used.

 

  • Updated radar sensor model

The radar sensor has been ported to the PreScan Multi-Processing architecture:

  • During simulation it will be run as a separate process resulting in a better performance.
  • Usage of multiple Radar sensors has improved. Multiple sensors can simulate in parallel instead of serially.
  • Small sensor quality improvements have been implemented.
  • Updated GIDAS plugin

Support was added for the import of lane marker patterns. Marker lines from the GIDAS data will result in LinePlacedMarkers in the PreScan scenario.

The import functionality can now be called from the PreScan Command-Line Interface (PreScan.CLI.exe) and thus be used as part of a Test Automation process.

  • General improvements
  • pathfollower autoconnect: All inputs of both Path Follower and Path Follower with Preview are automatically fully connected with the belonging blocks
  • Custom mesh definition: the precision of 3D models of Roads, Lane Markers and Lane Definition Lines can now be controlled from Experiment Settings. With this the user can influence the performance & accuracy
  • Contact sensor performance improvement for CarSim and dSpace vehicle dynamics: A high Simulation Core and Visual World update rate in the Simulation Scheduler is no longer needed. See Migration notes and the CarSim 3D Demo Template for example Simulation Scheduler settings. 
  • TIS sensor:
    • Additional values are reported for detected dopplervelocity.
    • The translation and rotation vector for the detected point are published in the TISData bus in Simulink.
    • Default near clipping plane set to 1m (better range accuracy by default).
      The communication with the sensor from Simulink has improved. 
Fraunhofer v2x plugin

PreScan V7.1.1

  • New physics based camera sensor model

The traditional RGB-based camera implementation created images limited to the visual spectrum. In contrast, the new PreScan spectral HDR camera model allows for high color depth, broad spectrum and physically correct image generation. The model simulates light in the 320-1500nm spectral range which traverses through the various media and lenses before the sensor model produces the final image signal. Other important features of this new spectral HDR camera model are a depth resolution of 20 bit per waveband as well as an increased dynamic range. 

 

  • Line Placed Marker

Lane Markers can now be added to Paths or to Road Segments. This makes it possible to add a repeated patterns of markers to a scenario at any location.

 

  • Fade and holes extended

Fade and holes can now also be applied to Road Markings, Priority Lines and Line Placed Markers.

 

  • Compilation Sheet Migration Dialog

For some PreScan blocks on the Compilation Sheet, the user can now choose whether the block is migrated (removing any user configuration) to the latest version of the PreScan block.

 

  • Traffic Sign imperfection editor

Traffic signs can be configured to have dirt (e.g. snow, mud) or scratches. The opacity and the amount of coverage can be specified.

 

  • GIDAS based PCM®  plugin

The GIDAS Importer is a plugin for the PreScan Experiment Editor. With the plugin it is possible to import cases out of the GIDAS based PCM® and it uses the information to build PreScan scenarios. The scenarios can then be used like any PreScan scenario, for example to study the effects of using an Advanced Driver Assistance System (ADAS) in such a scenario. For more information please see the documentation of the plugin.

 

  • LaneMarkerSensor

The LaneMarkerSensor has been improved with regard to performance. The performance of multiple LaneMarkerSensors in one experiment has been improved significantly. The slices of the LaneMarkerSensor are configurable.

PreScan V7.0

  • Intelligent Traffic Module (licensed separately)

The Intelligent Traffic Module (ITM) is a plug-in capable of generating traffic on a road network without the need to manually create paths and logic to keep traffic flowing. ITM controlled vehicles will find the routes over a network to get them from point A to point B.  Host vehicle algorithms can thus be subjected to a wide variety of traffic situations.

  • Remote Viewer

The Remote Viewer plug-in contains functionality to run viewer windows on different (networked) machines.

  • Selection Improvement

Object selection and manipulation in the build area was improved: Users can now select objects which are occluded by other objects using the selection list in the context menu. Users can manipulate objects using their borders. New, clear selection indication. New display mode – Wireframe mode.

  • Simple Dynamics Discrete-Time model

Besides a simple dynamics continuous-time model a discrete-time compilable model is now available

  • Korean traffic lights

Two new Korean traffic light models are added: Traffic Light Single (4 lamps) and Traffic Light Double (2x3 lamps).

  • Faded lane markers

Degraded lane markers pose  a great challenge to lane recognition algorithms. To be able to study the effect of wear and tear on these algorithms,  a new option is added to gradually fade the lane marker paint and to add random holes to the lane markers (i.e. wear and tear) .  

PreScan waer and tear
Faded lane markers

  • Lens map distortions

Different types of (fisheye) lenses and non-perfect lenses can be modeled with lens look up maps. With this feature end-users are able to model their own specific kind of lens, including any distortion and/or imperfections. The fisheye lens camera effect now has an option to save and load the lens map to / from an external file.

  • Lens overlay

Lens overlay is a related feature to lens maps and involve a post-processing step where a configurable bitmap is drawn over the rendered view. Hence dirt and other artifacts can be mimicked. Another use-case is to use the overlay to add text or warning signals over the rendered view. The overlay can be switched on/off from Simulink, supplying the user with the appropriate feedback when required.

  • Other enhancements
    • MATLAB 2013 a/b are now supported.
    • The LKAS Test scenarios are now available for MATLAB 2010 (a/b)
    • The User Interface and Visualization features for the V2X Scenarios have been updated to display more useful information.
    • The V2X_TC_Road Accident Scenario has been replaced with V2X_TC_CarBreakdownScenario to represent a more realistic real-life situation. 
    • The V2X_TC_RoadWorksWarning scenario has also been updated according to real-life V2X use cases.
    • The Mercedes Actros 1851 is now available with 3D Simple Dynamics. The actor is able to drive on 3D roads
PreScan lens distortions
Lens map distortions

PreScan V6.9

  • US traffic lights
    New US traffic light models are added: Traffic Light Single (US), Traffic Light Double (US), Traffic Light Double DogHouse (US).
  • Atmospheric sky model


    A physically-based analytical model of the daytime sky can now be used instead of using an image based sky. The HDR sky is generated according to turbidity, ground albedo and sun settings.
  • Path merging with preview
    A path connecting functionality is available to glue different paths together. Snap points will now appear and a snap-preview is shown.
  • 3D Basic Dynamics on banked road
    The 3D Basic Dynamics model is now enabled for all types of PreScan road profiles. 
  • Vehicular communication (V2X) demos
    A set of V2X demos have been added to the PreScan sample scenarios database. The following applications are available: Road Works Warning, Electronic Emergency Braking Light (EEBL), Green Light Optimal Speed Advisory (GLOSA), Signal Violation Warning. 
US traffic light

PreScan V6.8

  • Customizable road asphalt appearance
    Asphalt of road segments can be configured by user with standard texture, single color, color RGB texture, bumped texture and bumped wet texture.
  • Wall objects


    A new object representing a wall can be specified in the same way as a line placement or guardrail.
  • Line placements on paths
    Line placements can now be placed on every path as well as on road segments.
  • New 3D ramp properties
    The ramp segment has been enhanced with a constant slope property: Angle of Constant Slope and Length of Constant Slope 
  • Split and merge option for flexible roads
    Flexible roads can now be split into two separate parts and two flexible roads can be merged into one. This allows for easier manipulation of scenarios with many or long roads.
  • AEB Pedestrian demo including Euro NCAP AEB VRU scenarios
    The demonstrator showcases the use of PreScan for developing AEB Pedestrian systems. The Euro NCAP protocol scenarios for AEB VRU assesment are provided.
Improved sun and headight reflections using new asphalt implementations

PreScan V6.7

  • Distributed TIS Sensor
    TIS sensor calculations can now be distributed over different machines, CPU cores and/or GPU's. As a result the experiment run time can be reduced significantly.
  • Custom Marker Patterns


    Lane markers, curb markers and center line markers can now be configured to contain multiple independent marker patterns.
  • Motion Blur
    A velocity based motion blur camera effect is added. Depending on the object/camera speed, frame rate and shutter time, objects that move faster relative to the camera will appear more blurred.
  • Mirror reversal
    The user can use a normal camera as a mirror, by flipping the image horizontally. Applications include rear and side view mirrors
  • Auto-placement of guard rails
    An extra option is available to add guard rails to road segments as a type of line placement. They are extruded smoothly along any road shape
  • Traffic Sign Recognition and Intelligent Speed Assist demo including Euro NCAP scenarios
    The demonstrator showcases the use of PreScan for developing TSR and ISA systems. Protocol scenarios (Euro NCAP) and real-life scenarios are provided.
Example of custom marker patterns
Example of custom marker patterns

PreScan V6.6

  • Configurable road friction
    Configurable road friction coefficients for each road segment to be used for road-tyre contact calculations within the applied vehicle dynamics model. The friction coefficient can be exported to 3rd party vehicle model solvers such as CarSim, dSPACE ASM, etc.
  • Lane labels
    Numerical labels can be associated with lane, center and curb marker lines of road segments. The lane marker sensor is extended to report lane labels on the left and right of the actor. This new sensor output can be used to easily detect when a vehicle crosses to another driving lane.
PreScan urban scenario
PreScan urban scenario

PreScan V6.5

  • Enhanced coupling with CarSim vehicle dynamics
    The enhanced CarSim interface makes it possible to include detailed vehicle dynamics models from CarSIM software (Mechanical Simulation Corporation) in your PreScan simulations.The interface has been extended to support driving the CarSIM vehicle model on complex 3D road networks from PreScan (eliminating the need to model the same roads in CarSIM). 
  • Increased performance of path follower with preview
    The simulation time of applications which make use of the PreScan path follower with preview may reduce significantly.
  • SAE J2735 Basic Safety Message 2 (BSM part 2)
    In addition to the time-triggered position message BSM part 1, PreScan now also supports the event-driven hazard warning message BSM part 2. Since the BSM part 2 has optional elements, messages can be selected and deselected in the PreScan editor. Moreover, it is possible to differentiate the frequency of the data elements of BSM part 2.A new demo is included to demonstrate the use of both parts of the BSM.
PreScan - CarSim coupling
PreScan - CarSim coupling

PreScan V6.4

  • Improved performance of radar, lidar and ultrasonic sensor simulations
    Advanced GPU options are available to speed up the TIS sensor (used for radar, lidar, PMD and ultrasonic sensors). Speed improvements of factor 3-15 have been measured for user applications resulting in real-time performance. 
  • Euro NCAP AEB demo with city and inter-urban scenarios
    Ready-to-use Euro NCAP AEB scenarios are available to assess the effectiveness of the AEB system under different driving conditions. A balloon car model representing the target prescribed by the upcoming Euro NCAP AEB (Automatic Emergency Braking) protocol.
  • V2V demos for DSRC BSM Forward Collision Warning & Do Not Pass Warning
    These demos illustrate a Forward Collision Warning (FCW) application and Do Not Pass Warning (DNPW) application based on Vehicle-to-Vehicle (V2V) communication using Dedicated Short Range Wireless Communications (DSRC). The vehicles involved in the scenario use the Basic Safety Message (BSM) according to the SAE J2735 protocol, which is the standard for V2X communication in the USA.
  • Others
    Road banking available for flexible road segments
    Significant performance improvement for ACC and AEBS demos
    Ford Focus Wagon added to the standard vehicle database
Euro NCAP AEB demo with city and inter-urban scenarios
Euro NCAP AEB demo with city and inter-urban scenarios

PreScan V6.3

  • DSRC Receiver & Transmitter sensors with SAE J2735 BSM part1 message set
    Using the DSRC Receiver (Rx) andTransmitter (Tx) sensors, data between actors can be exchanged using a selected DSRC protocol andselected message types. Currently, the SAE J2735 protocol and its basic safety message (BSM) part 1 are supported. This is the standard for vehicle-to-vehicle (V2V) and vehicle-to-infrastructure (V2I) safety applications in the USA. 
  • EuroNCAP balloon car for AEB (Inter)urban testing
    A balloon car was added to the available models. It can be found under Actors - Targets. The balloon car represents the target prescribed by the upcoming Euro NCAP AEB (Automatic Emergency Braking) protocol.
  • New set of USA traffic signs
    USA traffic sign set has been complemented. The set contains new direction, transition and slope categories. The image quality has been improved, and new arrow-shape designs have been added. Also, all traffic signs are now retro-reflective allowing traffic sign recognition studies during night conditions.
USA traffic sign database
USA traffic sign database

PreScan V6.2

  • Object camera sensor
    The object camera sensor is a new camera sensor that provides target object information of scene elements on object level. It is used for ADAS algorithm development when image processing algorithms are not available and target object data cannot be derived from the PreScan camera images.
  • New shadow and light options for better CPU performance
    Different options for shadow calculations from sunlight are added. Different options for the definition of lights are added. Selection of the options will depend on the required need for detail or simulation efficiency.
  • 3D road banking
    Bank angles can now be defined for straight, bend, curved, ramp and spiral (clothoid) road segments.
  • Enhancements for Traffic Sign Recognition
    - German traffic sign set extended
    - Traffic signs are now retro-reflective allowing TSR night studies
    - Automated traffic sign import from OpenStreetMap
    - Large area network import from OpenStreetMap
  • Lane Departure Warning and Lane Keeping Assist demo including ISO and NHTSA scenario sets
    The demonstrator showcases the use of PreScan for developing LDW and LKA systems and provide protocol scenarios (ISO, NHTSA) and real-life scenarios for lateral guidance systems.
  • Pedestrian detection and avoidance demo
    The demonstrator showcases the use of PreScan for developing pedestrian detection and avoidance systems and provide a variety of challenging real-life scenarios
  • Coupling with dSPACE ASM vehicle models
    The dSPACE/ASM interface makes it possible to include detailed vehicle dynamics models from ASM vehicle models in the PreScan simulation.The interface has been extended to support driving the ASM vehicle model on complex 3D road networks from PreScan (eliminating the need to model the same roads in ASM).
Coupling with dSPACE ASM vehicle models
Coupling with dSPACE ASM vehicle models

PreScan V6.0

  • Fish eye camera
    A new camera sensor for modeling cameras with an ultra-wide angle lens (<360°) is now available. FOV, sensor size and image diameters can be specified.
  • Camera model updates
    - Barrel & pincushion distortion
    - Gaussian blur
    - Camera effects can be saved and re-used in different experiments.
    - Different cameras can have different effects (HDR, distortions, blur, vignetting, etc).
  • CAD import for IGES, STEP and 3DXML formats
    The importer of user-defined objects and actors is now able to read CAD formats (STEP, IGES and 3DXML) in addition to Collada formats.
  • Flexible road segment
    A new flexible road segment type enables the user to define a road with any number of definition points. It allows to easily create long stretches of road with many curves and bends.xle.
  • Standard scenario sets for 
    - AEBS ADAC performance tests
    - ACC ISO 15622:2002, ISO 22178:2009 and ISO/NP 22179
    - LDW NHTSA and ISO confirmation tests
  • Other enhancements
    - 3D vehicle dynamics for all database vehicles
    - Haptic feedback for steering console
    - Area color picker
    - Lane marker settings per lane line
    - PreScan time-history signals in MADPost postprocessor
Fisheye camera with rain
Fisheye camera with rain

PreScan V5.4

  • Light reflections
    Light reflections from vehicle lights or other active light sources on wet roads, vehicle surfaces (metallic paint) and reflective road objects.
  • Reflective road objects
    - Cat eyes
    - Botts' dotts
    - Guardrail reflectors
    - Reflective roadside poles & signs
  • Sensor visualization in 3D viewer
    Visualization of sensor beams is available for all sensor types (camera, radar, lidar, ultrasonic and V2x). Field of view, range and scan patterns can be visualized.
  • Vehicle dynamics for user-imported vehicle models
    PreScan vehicle dynamics properties can be assigned to vehicles that are imported via the user-defined library wizard. The wizard is extended to guide the user through the necessary steps.
  • New trailer type for truck modeling
    New trailer model with articulating shaft and front axle.
  • New AEBS and ACC demos in ADAS toolbox 
    - AEBS demonstrator for ADAC test scenarios
    - ACC with Stop & go for ISO test protocol
  • Support of dSPACE/ASM vehicle dynamics
    PreScan can now be used with dSPACE/ASM vehicle dynamics. The dSPACE/ASM interface makes it possible to include detailed vehicle dynamics from existing dSPACE/ASM models in the PreScan analysis.
  • Other enhancements
    - Occlusion option for bounding box ground-truth sensor
    - Smooth jerk option in speed profile editor
    - Support of Simulink acceleration mode
    - Sidewalks for all road segments
    - Automated import of road signs from OpenStreetMap database
Light reflections from vehicle lights
Light reflections from vehicle lights